Read-only |
About PNOP / PSAT Marker Search |
Description |
Returns the Pin result of a PNOP or PSAT marker search. PNOP In = Marker 4 X-axis value PSAT In = Marker 2 X-axis value |
VB Syntax |
pIn = pMark.Pin |
Variable |
(Type) - Description |
|
pIn |
(double) - Variable to store returned value |
|
pMark |
A PNOP (object) or PSaturation (object) |
Return Type |
Double |
Default |
Not applicable |
Examples |
pIn = pMark.Pin 'Read |
C++ Syntax |
HRESULT get_Pin(double* pNewVal) |
Interface |
IPNOP or IPSaturation |