Write/Read |
About External DC Devices |
Description |
Sets and returns the Point Read Commands for an external DC Meter or Point Set Commands for an external DC Source. |
VB Syntax |
extDC.PointCmd = value |
Variable |
(Type) - Description |
|
extDC |
An ExternalDCDevice (object) |
|
value |
(String) For DC Source, sets the Point Set Commands. Use {%f} to specify a double value and {%d} to specify an integer. For DC Meter, sets the Point Read Commands (for example, meas:volt?). |
Return Type |
String |
Default |
" " Empty String |
Examples |
extDC.PointCmd = "sour1:volt {%f}" 'Write |
|
value = extDC.PointCmd 'Read |
|
C++ Syntax |
HRESULT get_PointCmd(BSTR* cmd) HRESULT put_PointCmd(BSTR cmd) |
Interface |
IExternalDCDevice3 |