Write/Read |
About Fixturing |
Description |
Sets and returns the Real portion of the impedance value for the specified single-ended port. Use PortArbzImag to set the imaginary value. Or use PortArbzZ0 to set both values together. |
VB Syntax |
fixture.PortArbzReal(portNum) = value |
Variable |
(Type) - Description |
|
fixture |
A Fixturing (object) |
|
portNum |
(Integer) Single-ended port number to receive impedance value. |
|
value |
(Double) Real Impedance value. Choose a value between 0 to 1E7 |
Return Type |
Double |
Default |
50 |
Examples |
fixture.PortArbzReal(2) = 75 'Write |
|
value = fixture.PortArbzReal(1) 'Read |
|
C++ Syntax |
HRESULT get_PortArbzReal( short portNum, double *pVal) |
Interface |
IFixturing3 |