Read/Write |
|
Description |
Sets and reads the logic mode of Port C on the Handler IO connector. |
VB Syntax |
AuxIO.PortCLogic = value |
Variable |
(Type) - Description |
|
AuxIO |
(object) - A Hardware Aux I/O object |
|
value |
(Enum as NaRearPanelIOLogic) - Choose from: 0 - naPositiveLogic - The associated data line goes HIGH when writing a 1 to a PortC bit. 1 - naNegativeLogic - The associated data line goes LOW when writing a 1 to a PortC bit. When Port C is in Output/Write mode, a change in logic causes the output lines to change state immediately. For example, Low levels change to High levels. When Port C is in Input/Read mode, a change in logic will not cause the lines to change, but data read from Port C will reflect the change in logic. |
Return Type |
Enum |
Default |
1 - naNegativeLogic |
Examples |
auxIO.PortCLogic = value 'Write value = auxIo.PortCLogic 'Read |
C++ Syntax |
HRESULT put_PortCLogic ( tagNARearPanelIOLogic Mode ); HRESULT get_PortCLogic ( tagNARearPanelIOLogic* Mode ); |
Interface |
IHWAuxIO |