Read/Write |
|
Description |
Sets and reads whether Port C is setup for writing or reading data on the Handler IO connector. |
VB Syntax |
AuxIO.PortCMode = value |
Variable |
(Type) - Description |
|
AuxIO |
(object) - A Hardware Aux I/O object |
|
value |
(enum as NaPortMode) - Choose from: 0 - naInput - set the port for reading 1 - naOutput - set the port for writing |
Return Type |
Enum as NaPortMode |
Default |
1 - naInput |
Examples |
auxIo.get_PortCMode = naInput 'Write value = auxIo.get_PortCMode 'Read |
C++ Syntax |
HRESULT get_PortCMode( tagNAPortMode* pMode ); HRESULT put_PortCMode( tagNAPortMode pMode ); |
Interface |
IHWAuxIO |