Write/Read |
About Fixturing |
Description |
Sets and returns the Port Matching circuit model for the specified port number. Note: This command affects ALL measurements on the channel. |
VB Syntax |
fixture.PortMatchingCktModel(port) = value |
Variable |
(Type) - Description |
|
fixture |
A Fixturing (object) |
|
port |
(Integer) Port number to receive circuit model. |
|
value |
(Enum as NAFixturingPortMatchCkt) Circuit model. Choose from 0 naFixPMC_SLPC Series L - Parallel C 1 naFixPMC_PCSL Parallel C - Series L 2 naFixPMC_PLSC Parallel L - Series C 3 naFixPMC_SCPL Series C - Parallel L 4 naFixPMC_PLPC Parallel L - Parallel C 5 naFixPMC_USER Load S2P file - also set filename to load with strPortMatch_S2PFile Property 6 naFixPMC_NONE No circuit model 7 naFixPMC_SCPC Series C - Parallel C 8 naFixPMC_PCSC Parallel C - Series C 9 naFixPMC_SLPL Series L - Parallel L 10 naFixPMC_PLSL Parallel L - Series L |
Return Type |
Long Integer |
Default |
naFixPMC_NONE |
Examples |
fixture.PortMatchingCktModel(2) = naFixPMC_PLSC 'Write |
|
value = fixture.PortMatchingCktModel(1) 'Read |
|
C++ Syntax |
HRESULT get_PortMatchingCktModel(short port tagNAFixturingPortMatchCkt *pVal) |
Interface |
IFixturing |