Write / Read |
About Receiver Leveling |
Description |
Sets and reads the port number for power range data. When two sources are available in combiner mode, refer to the following table.
1 Indicates that the port requires option 224 or 423. |
||||||||||||||||||
VB Syntax |
powerRange.PortNumber = value |
||||||||||||||||||
Variable |
(Type) - Description |
||||||||||||||||||
|
powerRange |
A PowerRange (object) |
||||||||||||||||||
value |
(Integer) Port number for power range data. |
||||||||||||||||||
Return Type |
Integer |
||||||||||||||||||
Default |
Not Applicable |
||||||||||||||||||
|
|
powerRange.PortNumber = 3 'Write |
||||||||||||||||||
C++ Syntax |
HRESULT get_PortNumber(short* port); HRESULT put_PortNumber(short port); |
||||||||||||||||||
Interface |
IPowreRange |