Write/Read |
About Diff I/Q App |
Description |
Sets and reads the port to be used as a reference when controlling phase for the specified <port>. On the Source Configuration dialog under Phase, this is the Refer To setting. |
VB Syntax |
DIQ.PortReference (port) = value |
Variable |
(Type) - Description |
|
DIQ |
A Differential I/Q (object) |
|
port |
(String) Source port name. Use SourcePortNames to read a list of valid source ports. |
|
value |
(String) Reference port. Use SourcePortNames to return a list of valid port names. The two internal VNA sources are available ONLY at specific ports. For example on a 4-port PNA-X, the possible port pairings are: 1/3, 1/4, 2/3, or 2/4. Port 1 can NOT be paired with Port 2, and Port 3 can NOT be paired with Port 4. Learn more about these limitations. |
Return Type |
String |
Default |
Depends on <port> |
Examples |
oDIQ.PortReference("port 1") = "Port 3" |
|
Value = oDIQ.PortReference("port 2") 'Read |
|
C++ Syntax |
HRESULT get_PortReference(BSTR port, BSTR* PortReference); HRESULT put_PortReference(BSTR port, BSTR PortReference); |
Interface |
IDIQ |