Write/Read |
About Port Extensions |
Description |
Sets and returns the Port Extensions Velocity Factor value for the specified port number. Note: This command affects ALL measurements on the channel. |
VB Syntax |
fixture.PortVelocityFactor(port) = value |
Variable |
(Type) - Description |
|
fixture |
A Fixturing (object) |
|
port |
(Integer) Port number to receive velocity factor value. |
|
value |
(Double) Velocity Factor value. Choose a number between: 0 and 10 (.66 polyethylene dielectric; .7 PTFE dielectric) |
Return Type |
Double |
Default |
1 |
Examples |
fixture.PortVelocityFactor(2) = .6 'Write |
|
value = fixture.PortVelocityFactor(1) 'Read |
|
C++ Syntax |
HRESULT get_PortVelocityFactor(short port double *pVal) |
Interface |
IFixturing4 |