Write/Read |
About iTMSA |
Description |
Sets and reads the state of power offset as a fixture with True Mode balanced measurements. Learn more about iTMSA power and power offset. |
VB Syntax |
balStim.PowerAsFixture = value |
Variable |
(Type) - Description |
|
balStim |
A BalancedStimulus (object) |
|
value |
(Boolean) State of power offset as a fixture. False Offset is applied but is NOT included as a fixture in the output calculations. True Offset is applied and included as a fixture in the output calculations. |
Return Type |
Boolean |
Default |
False |
Examples |
balStim.PowerAsFixture = False 'Write var = balStim.PowerAsFixture 'Read |
C++ Syntax |
HRESULT get_PowerAsFixture (VARIANT_BOOL *bVal) HRESULT put_PowerAsFixture (VARIANT_BOOL bVal) |
Interface |
IBalancedStimulus |