Write/Read |
About Power Slope |
Description |
Sets or returns the Power Slope value. Power Slope function increases or decreases the output power over frequency. Units are db/GHz. For example: PowerSlope = 2 will increase the power 2db/1GHZ. |
VB Syntax |
object.PowerSlope = value |
Variable |
(Type) - Description |
|
object |
Channel (object) or CalSet (object) - Read-only property |
|
value |
(double) - Power Slope. Choose any number between -2 and 2. |
Return Type |
Double |
Default |
0 |
Examples |
chan.PowerSlope = 2 'Write |
|
pwrslp = chan.PowerSlope 'Read |
|
C++ Syntax |
HRESULT get_PowerSlope(double *pVal) |
Interface |
IChannel |CalSet3 |