Write/Read |
About Calsets |
Description |
Specifies if the source power cal in the calset linked to a measurement cal should be enabled or disabled with that cal. |
VB Syntax |
pref.PreferSourcePowerCalFromCalset = bool |
Variable |
(Type) - Description |
|
pref |
A Preferences (object) |
|
bool |
(Boolean) - Choose from: 0 - False - Disable source power cal in calset. 1 - True - Enable source power cal in calset. |
Return Type |
Boolean |
Default |
0 - False |
Examples |
pref.PreferSourcePowerCalFromCalset = False 'Write |
|
prefer = pref.PreferSourcePowerCalFromCalset 'Read |
|
C++ Syntax |
HRESULT put_PrefeSourcePowerCalFromCalset( VARIANT_BOOL prefPowerCal) HRESULT get_PrefeSourcePowerCalFromCalset( VARIANT_BOOL *prefPowerCal) |
Interface |
IPreferences |