Write/Read |
Description |
Sets and reads the device being controlled by the pulse generator output. |
VB Syntax |
obj.TriggerInType = value |
Variable |
(Type) - Description |
pulse |
A PulseGenerator (object) |
value |
(enum NAPulseGenToDevice) Choose from: 0 - ADC_TRIGGER - Enables offset pulses using ADC delay. 1 - RF_MODULATOR - Iindicates that the pulse signal is used to drive the RF modulator. Only one pulse generator output can be used to drive an RF source. If you try to set more than one pulse generator output to RF_MODULATOR, then the other one will be set to UserN (where "N" is the pulse generator number) 2 - ADC_ACTIVITY - (Pulse4 only) Pulse4 can also be set to monitor ADC activity. This selection outputs a signal on Pulse4 when the ADC is active. This is the same as Pulse4OutAsADCActivity. 3 - USER1 - Use Pulse1 to control a DUT, DC biases, or other signals. 4 - USER2 - Use Pulse2 to control a DUT, DC biases, or other signals. 5 - USER3 - Use Pulse3 to control a DUT, DC biases, or other signals. 6 - USER4 - Use Pulse4 to control a DUT, DC biases, or other signals. |
Return Type |
Enum |
Default |
RF_MODULATOR |
Exaamples |
pulse.PulseTimingDevice = RF_MODULATOR 'Write |
value = pulse.PulseTimingDevice 'Read the value |
|
C++ Syntax |
HRESULT get_PulseTimingDevice(enum
NAPulseGenToDevice *val); |
Interface |
IPulseGenerator6 |