Write/Read |
About SA Application |
Description |
Set and read the LO randomize state. |
VB Syntax |
sa.EnableRandomizedLO = value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Boolean) Choose from: 0 - OFF - LO Randomize is set to OFF. 1 - ON - LO Randomize is set to ON. |
Return Type |
Boolean |
Default |
1 |
Examples |
sa.EnbaleRandomizedLO = OFF Write |
|
value = sa.EnbaleRandomizedLO 'Read |
|
C++ Syntax |
HRESULT put_EnableRandomizedLO(VARIANT_BOOL bEnable); HRESULT get_EnableRandomizedLO(VARIANT_BOOL* bEnable); |
Interface |
ISpectrumAnalyzer |