Write/Read |
About Phase Control |
Description |
Write and read an array of ratioed power offsets. This allows the setting of arbitrary impedance, which is used for active load applications. The number of offset values must be the same as the number of data points. Use RatioedPowerCorrectionEnabled to use the offset values. |
VB Syntax |
phase.RatioedPowerCorrectionData(srcPort) = value |
Variable |
(Type) - Description |
|
phase |
A PhaseControl Object |
|
srcPort |
(Long Integer) Source port for which to make phase control settings. Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port |
value |
(Long values) Ratioed amplitude offset data array. |
Return Type |
Long data array |
Default |
Not Applicable |
Examples |
phase.RatioedPowerCorrectionData 1 = .1,.2,.3 ' Write 3 power offset values |
|
value = phase.RatioedPowerCorrectionData 2' Read |
|
C++ Syntax |
HRESULT get_RatioedPowerCorrectionData(long port, long* pVals); HRESULT put_RatioedPowerCorrectionData(long port, long newVals); |
Interface |
IPhaseControl |