Write/Read |
About Noise Figure Cal |
Description |
Set and read the method used to characterize the noise receivers. |
VB Syntax |
noise.RcvCharMethod = value |
Variable |
(Type) - Description |
|
noise |
A NoiseCal (object) |
|
value |
(string) Receiver characterization method. NOT case-sensitive. Choose from:
NOTE: The Power Meter selection is NOT allowed when the Noise Bandwidth is 8 MHz or 24 MHz. |
Return Type |
String |
Default |
"NoiseSource” |
Examples |
noise.RcvCharMethod = "PowerMeter"'Write |
|
receiverMethod = noise.RcvCharMethod 'Read |
|
C++ Syntax |
HRESULT get_RcvCharMethod(BSTR* pValue) HRESULT put_RcvCharMethod(BSTR pNewValue) |
Interface |
INoiseCal3 |