Write/Read |
About Gain Compression |
Description |
Set and read the DC readings at the compression point in the last iteration of a smart sweep. Taking only these DC readings improves measurement speed. |
VB Syntax |
gca.ReadDCAtCompression = value |
Variable |
(Type) - Description |
|
gca |
A GainCompression (object) |
|
value |
(Boolean) Choose from: True Enable reading DC value at compression point in the last iteration of a smart sweep. False Disable reading DC value at compression point in the last iteration of a smart sweep. |
Return Type |
Boolean |
Default |
False |
Examples |
gca.ReadDCAtCompression = True 'Write |
|
enable = gca.ReadDCAtCompression 'Read |
|
C++ Syntax |
HRESULT get_ReadDCAtCompression(VARIANT_BOOL* enable) HRESULT put_ReadDCAtCompression(VARIANT_BOOL enable) |
Interface |
IGainCompression5 |