Read/Write |
About the Handler I/O Connector |
Description |
Determines the control of Material Handler connector Pin 21. |
VB Syntax |
handler.ReadyForTriggerState = value |
Variable |
(Type) - Description |
|
handler |
(object) - A Handler I/O object |
|
value |
(boolean) False - Pin 21 is controlled by Output Port B7 True - Pin 21 is controlled by the Ready for Trigger signal |
Return Type |
Boolean |
Default |
False |
Examples |
handler.ReadyForTriggerState = False 'Write bState = handler.ReadyForTriggerState 'Read |
C++ Syntax |
HRESULT put_ReadyForTriggerState (BOOL *pVal); HRESULT get_ReadyForTriggerState (BOOL newVal); |
Interface |
IHWMaterialHandlerIO2 |