Read-only |
About External Trigger |
Description |
Checks if the PNA is ready for a hardware trigger. This command is not intended to be used in a dynamic triggering situation where the ready status is constantly changing. Instead, the expected use is a more static situation where you are expecting the PNA to transition from not ready to ready, and then wait for a trigger. The PNA is polled until it becomes ready and then an operation that triggers the PNA is performed. Note: This command is only supported on the PNA-L, PNA, and PNA-X with DSP5 installed. Any other model will return an error. |
VB Syntax |
value = trigsetup.ReadyForTriggerStatus |
Variable |
(Type) - Description |
|
trigsetup |
A TriggerSetup (object) |
|
value |
(Enum as NATriggerReadyStatusSource) 0 - naTriggerAny - Check if the PNA is ready for any of the following hardware triggers. 1 - naTriggerMeas - Check if the PNA is ready for an External trigger from the Meas Trig In BNC, Handler IO Pin 18, or Pulse 3 line. 2 - naTrigger Aux1 - Check if the PNA is ready for a trigger from the AUX TRIG 1 IN on the rear panel. 3 - naTriggerAux2 - Check if the PNA is ready for a trigger from the AUX TRIG 2 IN on the rear panel. |
Return Type |
Boolean |
Default |
Not applicable |
|
|
value = trigsetup.ReadyForTriggerStatus 0 'Read |
C++ Syntax |
HRESULT get_ReadyForTriggerStatus(tagNATriggerReadyStatusSource whichTrigger, VARIANT_BOOL* val); |
Interface |
ITriggerSetup4 |