Read only |
About Receiver Temp |
Description |
Returns the current temperature on the VNA receiver board. |
VB Syntax |
value = cap.ReceiverTemperature (unit) |
Variable |
(Type) - Description |
|
value |
(Double) - Variable to store the returned temperature value. |
|
cap |
A Capabilities (object) |
|
unit |
(Enum as NATempScale) - Units in which temperature is returned. Choose from:
|
Return Type |
Double |
Default |
Not Applicable |
Examples |
value = cap.ReceiverTemperature naTempScale_Celsius'Read |
C++ Syntax |
HRESULT get_ReceiverTemperature(NATempScale val, long temperature); |
Interface |
ICapabilities9 |