Write/Read |
About Active Match |
Description |
Set and read the tone power relative to the input power (dBc). |
VB Syntax |
HotS22.RelativeExtractionToneLevel = level |
Variable |
(Type) - Description |
|
HotS22 |
A ActiveParametersApp (object) |
|
level |
(Double) - Relative tone power level |
Return Type |
Double |
Default |
-15 dBc |
Examples |
HotS22.RelativeExtractionToneLevel = -5 'Write |
|
level = HotS22.RelativeExtractionToneLevel 'Read |
|
C++ Syntax |
HRESULT get_RelativeExtractionToneLevel(double* level) HRESULT put_RelativeExtractionToneLevel(double level) |
Interface |
IActiveChannelSettings |