Write/Read |
About Safe Sweep |
Description |
Set and read the Safe Sweep FINE power adjustment. |
VB Syntax |
gca.SafeSweepFinePowerAdjustment = value |
Variable |
(Type) - Description |
|
gca |
A GainCompression (object) |
|
value |
(Double) Fine power adjustment setting in dBm. Choose a value from +30 to (-30). |
Return Type |
Double |
Default |
1.0 |
Examples |
gca.SafeSweepFinePowerAdjustment = 0.1 'Write |
|
SSfine = gca.SafeSweepFinePowerAdjustment 'Read |
|
C++ Syntax |
HRESULT get_SafeSweepFinePowerAdjustment(double* value) HRESULT put_SafeSweepFinePowerAdjustment(double value) |
Interface |
IGainCompression |