Write/Read |
About Safe Sweep |
Description |
Set and read the compression level at which Safe Sweep changes from the COARSE power adjustment to the FINE power adjustment. |
VB Syntax |
gca.SafeSweepFineThreshold = value |
Variable |
(Type) - Description |
|
gca |
A GainCompression (object) |
|
value |
(Double) Threshold setting in dBm. Choose a value from +30 to (-30). |
Return Type |
Double |
Default |
0.5 dBm |
Examples |
gca.SafeSweepFineThreshold = 0.1 'Write |
|
SSThresh = gca.SafeSweepFineThreshold 'Read |
|
C++ Syntax |
HRESULT get_SafeSweepFineThreshold(double* value) HRESULT put_SafeSweepFineThreshold(double value) |
Interface |
IGainCompression |