Read-only |
About GCA |
Description |
Returns a comma-separated list of the frequency indexes that were out of tolerance for SMART Sweep mode, or at the power limit for 2D Sweep mode. Zero (0) is the first frequency data point. Must be Single triggered. Invalid results occur if the GCA channel is continuously sweeping. |
VB Syntax |
value = gca.SearchFailures |
Variable |
(Type) - Description |
|
value |
(Double) Variable to store the returned data. |
|
gca |
A GainCompression (object) |
Return Type |
Returns a comma-separated list of frequency indexes. |
Default |
Not applicable |
Examples |
SFA = gca.SearchFailures 'Read |
C++ Syntax |
HRESULT get_SearchFailures(VARIANT* value) |
Interface |
IGainCompression |