Write/Read |
About SA Application |
Description |
Set and read the minimum search frequency to use during an Occupied BW search measurement. Power below this frequency is ignored. |
VB Syntax |
sa.SearchOccupiedBWMinFreq = value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Double) Minimum search frequency value. |
Return Type |
Double |
Default |
250 MHz |
Examples |
sa.SearchOccupiedBWMinFreq = 300e6 Write |
|
value = sa.SearchOccupiedBWMinFreq 'Read |
|
C++ Syntax |
HRESULT put_SearchOccupiedBWMinFreq(double minfreq); HRESULT get_SearchOccupiedBWMinFreq(double* minfreq); |
Interface |
ISpectrumAnalyzer4 |