Write/Read |
About Marker Search |
Description |
Emulates the Tracking function in the marker search dialog box. The value you choose for SearchFunction will determine the type of search that takes place when the Tracking property is set true. The tracking function finds the selected search function every sweep. In effect, turning Tracking ON is the same as executing one of the "Search..." methods (such as SearchMin, SearchMax) for every sweep. |
VB Syntax |
mark.SearchFunction = value |
Variable |
(Type) - Description |
|
mark |
A Marker (object) |
|
value |
(enum NAMarkerFunction) - search function. Choose from: 0 - naMarkerFunction_None 1 - naMarkerFunction_Min 2 - naMarkerFunction_Max 3 - naMarkerFunction_Target 4 - naMarkerFunction_NextPeak 5 - naMarkerFunction_PeakRight 6 - naMarkerFunction_PeakLeft 7 - naMarkerFunction_Compression |
Return Type |
Long Integer |
Default |
0 - naMarkerFunction_None |
Examples |
mark.SearchFunction = naMarkerFunction_Target 'When this marker is set to track, it will track the Target value. |
|
searchfunction = mark.SearchFunction 'Read |
|
C++ Syntax |
HRESULT get_SearchFunction(tagNAMarkerFunction *pVal) |
Interface |
IMarker |