Write/Read |
About Mixer/Converter Settings |
Description |
Sets and returns the number of data points to be measured in the sweep segment. Send Apply before sending a query (read). Learn more. |
VB Syntax |
conv.SegmentPoints(index) = value |
Variable |
(Type) - Description |
|
conv |
|
|
index |
(Long integer) Segment for which points is to be set. Choose a segment between 1 and the current segment count. Use SegmentCount Property to read the current count in the Applied Mixer. |
|
value |
(Long integer) - Choose a value between 1 and the maximum number of data points allowed in the VNA. This is also the total number of points allowed for ALL segments. |
Return Type |
Long integer |
Default |
21 |
Examples |
mxr.SegmentPoints(1)=3 'Sets 3 points for segment 1. |
C++ Syntax |
HRESULT get_SegmentPoints(long index, long * val); HRESULT put_SegmentPoints(long index, long val); |
Interface |
IConverter5 |