Write/Read |
About Mixer/Converter Settings |
Description |
Sets or returns the segment sweep mode (Swept or Fixed) for the specified range (Input/LO/Output). Send Apply before sending a query (read). Learn more. |
VB Syntax |
conv.SegmentRangeMode(index,range) = value |
Variable |
(Type) - Description |
|
conv |
|
|
index |
(Long integer) Segment for which mixing mode being set. Choose a segment between 1 and the current segment count. Use SegmentCount Property to read the current count in the Applied Mixer. |
|
range |
(Enum as ConverterFrequencyRange) Range for which sweep mode is being set. Choose from: 0 - naInputFrequencies - set input sweep mode. 1 - naOutputFrequencies - set output sweep mode. 2 - naLO1Frequencies - set LO1 sweep mode. 3 - naLO2Frequencies - set LO2 sweep mode. 4 - naIFFrequencies - set IF sweep mode. |
|
value |
(Enum as NARangeMode) Choose from: 0 - naSwept Range is swept 1 - naFixed Range is fixed. |
Return Type |
Enum as NARangeMode |
Default |
Input and Output - naSwept LO (1 and 2) - naFixed |
Examples |
mxr.SegmentRangeMode(1,1)=0 'sets segment 1 output range to swept. |
C++ Syntax |
HRESULT get_SegmentRangeMode(long index, tagConverterFrequencyRange range, tagNARangeMode *value); HRESULT put_SegmentRangeMode(long index, tagConverterFrequencyRange value, tagNARangeMode value); |
Interface |
IConverter5 |