Read-only |
About SA Application |
Description |
Read the current span DFT bin count, the number of DFT points processed across the total RF span. When the Detector is bypassed, this is the number of points that are sent to the display. |
VB Syntax |
value = sa.SpanBinsCount |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Long) Variable to store the returned value. |
Return Type |
Long |
|
Example |
value = sa.SpanBinsCount'Read |
C++ Syntax |
HRESULT get_SpanBinsCount(long* val); |
Interface |
ISpectrumAnalyzer4 |