Write/Read |
About SA Application |
Description |
Set and read the Frequency Span / RBW ratio. |
VB Syntax |
sa.SpanResolutionBWRatio = value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Double) Frequency Span / RBW ratio. Choose a value between 1 and 200e9. |
Return Type |
Double |
Default |
106 |
Examples |
sa.SpanResolutionBWRatio = 100 Write |
|
value = sa.SpanResolutionBWRatio 'Read |
|
C++ Syntax |
HRESULT put_SpanResolutionBWRatio(double ratio); HRESULT get_SpanResolutionBWRatio(double* ratio); |
Interface |
ISpectrumAnalyzer |