Write/Read |
About Power Sweep |
Description |
Sets the start power of the analyzer when sweep type is set to Power Sweep. Frequency of the measurement is set with chan.CWFrequency. |
VB Syntax |
object.StartPower = value |
Variable |
(Type) - Description |
|
object |
One of the following: |
|
value |
(double) - Start Power in dBm. Note: The range of settable power values depends on the VNA model and if source attenuators are installed. To determine the range of values, use cap.MaximumSourceALCPower and cap.MinimumSourceALCPower Auto attenuation is not allowed in Power Sweep. |
Return Type |
Double |
Default |
0 |
Examples |
Chan.StartPower = -10 'Write |
|
strtpwr = Chan.StartPower 'Read |
|
C++ Syntax |
HRESULT get_StartPower(double *pVal) |
Interface |
IChannel |CalSet3 |