Write/Read |
Description |
Turns an Object ON and OFF. |
|
VB Syntax |
object.State = value |
|
Variable |
(Type) - Description |
|
|
object |
Applies to any of the following objects: Port Extension- Superseded. See either:
|
|
|
value |
(boolean) - False - Turns obj OFF True - Turns obj ON |
|
Return Type |
Boolean |
|
Default |
Depends on the object: 0 - FOM 0 - Gating 0 - InterfaceControl 0 - LimitTest 1 - Segment 0 - Transform 0 - Equation 0 - FIFO |
|
Examples |
Seg.State = 1 'Turns the segment object ON -Write |
|
|
tran = Trans.State 'returns the state of Transform -Read |
||
C++ Syntax |
HRESULT get_State(VARIANT_BOOL *pVal) |
|
Interface |
ISegment IInterfaceControl ITransform IGating ILimitTest IFOM IEquation IEmbeddedLO IFIFO |