Write/Read |
Description |
Turns the specified pulse generator ON and OFF. |
VB Syntax |
pulse.State (n) = value |
Variable |
(Type) - Description |
|
pulse |
A PulseGenerator (object) |
|
n |
(Integer) Pulse generator number. Choose from 0 to 4. Or use PulseGeneratorID to refer to an external pulse generator. 0 is the generator that pulses the ADC. |
|
value |
True - turns pulse output ON. False - turns pulse output OFF. |
Return Type |
Boolean |
Default |
False |
Examples |
pulse.State(1) = True 'Write |
|
value = pulse.State(4) 'Read |
|
C++ Syntax |
HRESULT get_State(integer pulse, VARIANT_BOOL *pVal); HRESULT put_State(integer pulse, VARIANT_BOOL newVal); |
Interface |
IPulseGenerator |