Write/Read |
About User Ranges |
Description |
Sets the User Range number for calculating measurement statistics. Set the start and stop values for a User Range with UserRangeMin and UserRangeMax. There are 16 User Ranges per channel. User ranges are applied independently to any measurement. |
VB Syntax |
meas.StatisticsRange = value |
Variable |
(Type) - Description |
|
meas |
A Measurement (object) |
|
value |
(long integer) - Range Number. Choose any number between 0 and 16 0 is Full Span 1 - 16 are user-defined ranges |
Return Type |
Long Integer |
Default |
0 |
Examples |
meas.StatisticsRange = 2 'Write |
|
statrange = meas.StatisticsRange 'Read |
|
C++ Syntax |
HRESULT get_StatisticsRange(long* rangeNumber) |
Interface |
IMeasurement |