Read-only |
About Cal Sets |
Description |
Returns the specified X-axis FOM frequency range. The array contains one frequency value for each data point. |
VB Syntax |
value = calSet.StimulusValues (range) |
Variable |
(Type) - Description |
|
calSet |
CalSet (object) - Read-only property |
|
range |
(Long) FOM frequency range to read. 0 - returns source frequencies. 1 - returns response frequencies. 2 - returns primary frequencies. |
Return Type |
1-dimensional variant array |
Default |
Not Applicable |
Examples |
array = CalSet.StimulusValues 'Read |
C++ Syntax |
HRESULT get_StimulusValues (long range, VARIANT* vals) |
Interface |
ICalSet3 |