Read- only |
|
Description |
Returns the stimulus value of the last data point for the measurement. To understand how this property is useful, see IMeasurement2 Interface. |
VB Syntax |
value = meas.Stop |
Variable |
(Type) - Description |
|
value |
(Double) Variable to store the returned value |
|
meas |
A Measurement (object) |
Return Type |
Double |
Default |
Not Applicable |
Examples |
Print meas.Stop 'prints the stimulus value of the last data point |
C++ Syntax |
HRESULT get_Stop(double * Val); |
Interface |
IMeasurement2 |