Description |
Sets and reads the event that will cause the Sweep End line to go to a low state. The line will return to a high state after the appropriate calculations are complete. Note: This line is connected to the HANDLER IO connector. |
VB Syntax |
object.SweepEndMode = value |
Variable |
(Type) - Description |
|
object |
(object) - A HandlerIO or AuxIO object |
|
value |
(enum as NASweepEndMode ) Choose from: 0 - naSweep - the line goes low when each sweep is complete 1 - naChannelSweep - the line goes low when all the sweeps for each channel is complete. 2 - naGlobalSweep - the line goes low when all sweeps for all triggerable channels are complete. |
Return Type |
Long Integer |
Default |
0 - naSweep |
Examples |
HWAuxIO.PassFailMode = naSweep 'Write value = HWAuxIO.PassFailMode 'Read |
C++ Syntax |
HRESULT put_SweepEndMode ( tagNASweepEndMode Mode ); HRESULT get_SweepEndMode ( tagNASweepEndMode* Mode ); |
Interface |
IHWAuxIO IHWMaterialHandlerIO |