Write/Read |
About Stepped Sweep |
Description |
Sets the method used to generate a sweep: continuous ramp (analog) or discrete steps (stepped). |
VB Syntax |
object.SweepGenerationMode = value |
Variable |
(Type) - Description |
|
object |
Channel (object) or CalSet (object) - Read-only property |
|
value |
(enum NASweepGenerationModes) - Choose either: 0 - naSteppedSweep - source frequency is CONSTANT during measurement of eah displayed point. More accurate than Analog. Dwell time can be set in this mode. 1 - naAnalogSweep - source frequency is continuously RAMPING during measurement of each displayed point. Faster than Stepped. Sweep time (not dwell time) can be set in this mode. |
Return Type |
Long Integer |
Default |
Analog |
Examples |
Chan.SweepGenerationMode = naAnalogSweep 'Write |
|
swpgen = Chan.SweepGenerationMode 'Read |
|
C++ Syntax |
HRESULT get_SweepGenerationMode(tagNASweepGenerationModes* pVal) |
Interface |
IChannel |CalSet3 |