Write/Read |
About Marker Search |
Description |
Sets the target value for the marker when doing Target Searches (SearchTargetLeft, SearchTarget, SearchTargetRight). |
VB Syntax |
mark.TargetValue = value |
Variable |
(Type) - Description |
|
mark |
A Marker (object) |
|
value |
(single) - Target value. Choose any number between: -500 and 500 |
Return Type |
Single |
Default |
0 |
Examples |
mark.TargetValue = 10.5 'Write |
|
target = mark.TargetValue 'Read |
|
C++ Syntax |
HRESULT get_TargetValue(float *pVal) |
Interface |
IMarker |