Write/Read |
About External Devices |
Description |
Sets and returns the Time out value for communication with the external device. An error is returned if communication with the device is not successful within this period of time. |
VB Syntax |
extDevices.TimeOut = value |
Variable |
(Type) - Description |
|
extDevices |
An ExternalDevice (object) |
|
value |
(Double) Time out in milliseconds. |
Return Type |
Double |
Default |
20000 milliseconds (20 seconds) |
Examples |
extDevices.TimeOut = 1000 Write value = extDevices.TimeOut 'Read |
C++ Syntax |
HRESULT get_TimeOut(Double* value); HRESULT put_TimeOut(Double newVal); |
Interface |
IExternalDevices |