Write/Read |
About Trace Hold |
Description |
Sets the type of trace hold operation to perform. |
VB Syntax |
meas.TraceHoldType = value |
Variable |
(Type) - Description |
|
meas |
A Measurement (object) |
|
value |
(Enum as NATraceHoldType) - Choose from: naTraceHoldOff - Disables the Trace Hold feature. naTraceHoldMinimum - Sets Trace Hold to store the lowest measured data points. naTraceHoldMaximum - Sets Trace Hold to store the highest measured data points. |
Return Type |
Enum |
Default |
naTraceHoldOff |
VB Examples |
meas.TraceHoldType = naTraceHoldOff 'Write |
|
hold = meas.TraceHoldType 'Read |
|
C++ Syntax |
HRESULT get_TraceHoldType(tag NATraceHoldType *pVal) HRESULT put_TraceHoldType(tag NATraceHoldType newVal) |
Interface |
IMeasurement16 |