Write/Read |
About Triggering ADC |
Description |
Set and read the ON/OFF state of a measurement trigger event that will occur whenever the ADC level is greater than the value specified using the TriggerADCLevelValue command. |
VB Syntax |
sa.TriggerADCLevelState = value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Boolean) Choose from: 0 - OFF - ADC measurement trigger OFF. 1 - ON - ADC measurement trigger ON. |
Return Type |
Boolean |
Default |
0 |
Examples |
sa.TriggerADCLevelState = OFF Write |
|
value = sa.TriggerADCLevelState 'Read |
|
C++ Syntax |
HRESULT put_TriggerADCLevelState(VARIANT_BOOL bEnable); HRESULT get_TriggerADCLevelState(VARIANT_BOOL* bEnable); |
Interface |
ISpectrumAnalyzer |