Write/Read |
About Triggering ADC |
Description |
Set and read the ADC trigger level. |
VB Syntax |
sa.TriggerADCLevelValue = value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Long) Choose a value between 0 and 16383. |
Return Type |
Long |
Default |
100 |
Examples |
sa.TriggerADCLevelValue = 256 'Write |
|
value = sa.TriggerADCLevelValue 'Read |
|
C++ Syntax |
HRESULT put_TriggerADCLevelValue(long val); HRESULT get_TriggerADCLevelValue(long* val); |
Interface |
ISpectrumAnalyzer |