Write/Read |
About Ext DC Devices |
Description |
When Trigger mode is set to Hardware List for SMU devices, this command sets and returns the B2900 Digital IO pin to use for Trigger IN. |
VB Syntax |
extDC.TriggerInPin = value |
Variable |
(Type) - Description |
|
extDC |
An ExternalDCDevice (object) |
|
value |
(Long) Pin number for Trigger IN. Choose a pin number from 1 to 14. |
Return Type |
Long |
Default |
1 |
Examples |
extDC.TriggerInPin = 3 'Write |
|
bool = extDC.TriggerInPin 'Read |
|
C++ Syntax |
HRESULT get_TriggerInPin (Long *pValue) HRESULT put_TriggerInPin (long newVal) |
Interface |
IExternalDCDevice2 |