Write/Read. |
About Trigger |
Description |
Use AUX.Enable to enable AUXI/O triggering. Use Trigger Source= External to enable Meas Trig Ready output. Enables the VNA to send trigger signals out the rear-panel TRIGGER OUT connector. |
VB Syntax |
trigsetup.TriggerOutputEnabled = boolean |
Variable |
(Type) - Description |
|
trigsetup |
A TriggerSetup2 (object) |
|
boolean |
Choose from: False - VNA does NOT send output trigger signals. True - VNA sends output trigger signals. |
Return Type |
Boolean |
Default |
False |
Examples |
trigsetup.TriggerOutputEnabled = True 'Write |
|
atba = trigsetup.TriggerOutputEnabled 'Read |
|
C++ Syntax |
HRESULT get_TriggerOutputEnabled( BOOL *pVal); HRESULT put_TriggerOutputEnabled( BOOL newVal); |
Interface |
ITriggerSetup2 |