Write/Read |
About Periodic Counter |
Description |
Set and read the ON/OFF state of a measurement trigger event based on the specified period set using the TriggerPeriodicCounterValue command. |
VB Syntax |
sa.TriggerPeriodicCounterState = value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Boolean) Choose from: 0 - OFF - Periodic counter OFF. 1 - ON - Periodic counter ON. |
Return Type |
Boolean |
Default |
0 |
Examples |
sa.TriggerPeriodicCounterState = OFF Write |
|
value = sa.TriggerPeriodicCounterState 'Read |
|
C++ Syntax |
HRESULT put_TriggerPeriodicCounterState(VARIANT_BOOL bEnable); HRESULT get_TriggerPeriodicCounterState(VARIANT_BOOL* bEnable); |
Interface |
ISpectrumAnalyzer |