Write/Read |
About ExternalDevices |
Description |
Sets and returns the VNA port through which an external source is to be triggered. |
VB Syntax |
extSource.TriggerPort = value |
Variable |
(Type) - Description |
|
extSource |
An ExternalSource Object (object) |
|
value |
(enum NAExtDevTriggerPort) - Choose from: 0 - naExtDevTriggerPortBNC1 (VNA 'C' models) 1 - naExtDevTriggerPortAux1 (PNA-X models) 2 - naExtDevTriggerPortAux2 (PNA-X models) |
Return Type |
Enum |
Default |
For VNA 'C' models - BNC1 For PNA-X models - Aux1 |
Examples |
extSource.TriggerPort = 1 'Write |
|
trigpt = extSource.TriggerPort 'Read |
|
C++ Syntax |
HRESULT get_TriggerPort (tagNAExtDevTriggerPort *pValue) |
Interface |
IExternalSource |