Write/Read |
About Sensor Cal Factors |
Description |
Enables/disables use of internal calibration factors for power sensors with built-in calibration factors and reads the current state. |
VB Syntax |
pwrSensor.UseInternalCalFactors = state |
Variable |
(Type) - Description |
|
pwrSensor |
A PowerSensorAsReceiver (object) |
|
state |
(boolean) False - Disables the use of internal calibration factors. True - Enables the use of internal calibration factors. |
Return Type |
Boolean |
Default |
False |
Examples |
' This example script demonstrates the set/get of the 'UseInternalCalFactors' property ' on the PMAR PowerSensor COM object for an existing PMAR named 'MyPMAR'. Option Explicit dim app Set app = CreateObject("AgilentPNA835x.Application") app.Preset app.ActiveChannel.Hold True app.ActiveChannel.CWFrequency = 1E9 app.ActiveChannel.SweepType = 3 'naCWTimeSweep app.ActiveChannel.NumberOfPoints = 3 dim externalDevices Set externalDevices = app.ExternalDevices dim externalDevice Set externalDevice = externalDevices.Item("MyPMAR") externalDevice.Active = True 'Create a PMAR trace with power sensor connected to port 3 app.ActiveMeasurement.ChangeParameter "MyPMAR", 3 dim PMAR Set PMAR = externalDevice.ExtendedProperties ' Disable use of the sensor's internal cal factors, take a sweep and report the Mean PMAR.UseInternalCalFactors = False externalDevice.IOEnable = True app.ActiveChannel.Single True MsgBox "UseInternalCalFactors = " & PMAR.UseInternalCalFactors & ", Mean measured val = " & app.ActiveMeasurement.Mean ' Enable use of the sensor's internal cal factors, take another sweep and report the Mean again externalDevice.IOEnable = False PMAR.UseInternalCalFactors = True externalDevice.IOEnable = True app.ActiveChannel.Single True MsgBox "UseInternalCalFactors = " & PMAR.UseInternalCalFactors & ", Mean measured val = " & app.ActiveMeasurement.Mean |
C++ Syntax |
HRESULT get_UseInternalCalFactors(VARIANT_BOOL *pVal) HRESULT put_UseInternalCalFactors(VARIANT_BOOL Val) |
Interface |
IPowerSensorAsReceiver3 |