Read-only |
About Path Configurator |
Description |
Returns an array of valid settings that can be used with the element object. See a list of configurable elements and settings for various VNA models. |
VB Syntax |
values = pathElement.Values |
Variable |
(Type) - Description |
|
values |
(Variant array) Variable to store the array of valid settings for the element. |
|
pathElement |
A PathElement (object) |
Return Type |
Variant array |
Default |
Not Applicable |
Examples |
settings=pathElement.Values |
C++ Syntax |
HRESULT Values( VARIANT* pValues ); |
Interface |
IPathElement |