Write/Read |
About Arranging Windows |
Description |
Sets or returns the window setting of Maximized, Minimized, or Normal. To arrange all of the windows, use app.ArrangeWindows. |
VB Syntax |
object.WindowState = value |
Variable |
(Type) - Description |
|
object |
An Application (object) - main window |
|
value |
(enum NAWindowStates) - The window state. Choose from: |
Return Type |
Long Integer |
Default |
naMaximized |
Examples |
app.WindowState = naMinimized 'changes the Network Analyzer application window to an icon. -Write |
|
winstate = app.WindowState 'Read |
|
C++ Syntax |
HRESULT get_WindowState(tagNAWindowStates *pVal) |
Interface |
INAWindow |